STM32Cube Programmer with STM32L522 bootloader run after programming
Hi,
I'm using the internal bootloader of the STM32L522 with STM32Cube Programmer to upload code via UART. I can upload new code without any issues. The problem is that I need the application to start after the programming is complete. I have the "Run after programming" box checked, but it doesn't start after the programming is complete. I have tried the same process using the STM32F411 and the application starts after programming. I'm very new to STM32 microcontrollers and would greatly appreciate any help I can get.