STM32CubeProgramme can connect after full flash erase of STM32H563 (NUCLEO-H563ZI)
Had been able to connect to connect to the STM32H563 chip using the STMCubeProgrammer. However after a full chip erase was performed was no longer able to connect. The following message popup appears when trying to connect:
“Cannot connect to access port1!. If you are trying to connect to a device with TrusZone enabled please try to connect with HotPlug mode. If you are trying to connect to H5 device and your target is already locked with password or certificate, please open your device using Debug Authentication."
Other than the full flash erase, no other operation was performed, no flash code had been changed, etc. The board was just out of the box working until the flash erase operation was performed.