STM32F070RBT6 RESET CONDITION
We work with STM32F070RBT6 . There is an internal POR/PDR controller in microcontroller but it seems to be active when VDD below 1.8V according to the product datasheet but the operating voltage seems between 2.4V to 3.6 V.
In Run Mode, If the input voltage VDD fall below 2.4V but not below VDR detect level (1.8.. 2V), in other words between (2.4 V and 2V) what will be happen?