STM32F1 I2C DMA has no stop bit
Hi. First time using this forum.
I'm using an STM32F103C8 (genuine, not bluepill clone).
I've easily used DMA to take sensor data and store it in a buffer, this has worked without issue (see below):
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin) {
if (GPIO_Pin == ACC_INT_Pin) // If The INT Source Is ACC
{
HAL_I2C_Mem_Read_DMA(&hi2c1, addr_LSM6 << 1, LSM6DS3_ACC_GYRO_OUTX_L_G,
I2C_MEMADD_SIZE_8BIT, mydata, 12);
}
}
However, when using the below code, it does not deliver the stop bit, resulting in all future transactions not working.
HAL_I2C_Mem_Write_DMA(&hi2c1, addr_LSM6 << 1, LSM6DS3_ACC_GYRO_CTRL9_XL, I2C_MEMADD_SIZE_8BIT, (uint8_t[] ) { 0x38 }, 1);
Using the exact same code in blocking mode (as below) works fine.
HAL_I2C_Mem_Write(&hi2c1, addr_LSM6 << 1, LSM6DS3_ACC_GYRO_CTRL9_XL,
I2C_MEMADD_SIZE_8BIT, (uint8_t[] ) { 0x38 }, 1, 1);
Here is a LA shot of the transaction:

As you can see, the SCL line is left high, and the transaction thus does not terminate properly. I should note that the data is received without issue.
Below is my cube configuration:


A similar issue also occurs when trying to read data in some cases, using this code:
uint8_t bmp280_interface_iic_read(uint8_t addr, uint8_t reg, uint8_t *buf, uint16_t len) {
uint8_t retval = HAL_I2C_Mem_Read_DMA(&hi2c1, addr, reg, 0x00000001U, buf, len);
return retval;
}
The stop bit is not generated, future transactions don't work as the SCL was not returned to high, though the data from that specific transaction is received without issue.
I should also stress that DMA works perfectly fine for the interrupt-triggered code I showed at the beginning.
In summary, my I2C DMA does not generate stop bits, but only for some code. It works fine in other cases. I have no clue what's going on here. Thanks.