STM32F101C8 Boot Loader reload?
Hello,
New here. I am working with a piece of consumer electronics equipment that uses a STM32F101C8 processor. the customer was doing an update to this unit and in the middle of the update, pulled the USB plug out of his computer bricking the unit. all attempts at using the manufacturers method of updating have failed. I have checked powers and grounds and all voltages are where they should be.
I have ordered a ST Link V2 programmer that is due today. I am looking for advice/info On How to get a baseline. How to connect and erase the chip back to a stock setting essentially. reload a basic boot loader. something to attempt to get the chip back to a basic state so i can re-attempt the update process.
I have the .BIN file from the MFG if that helps.
My thinking is that if i can connect, get in, set up a basic starting point. even something like the blink program would probably reset the chip enough for the manufactures update process through the ST software and USB converter would work. it is a last ditch hail mary pass before we replace a very expensive board.
there just has to be a way to do this without replacing the whole board. I SHOULD be able to re flash the MCU one way or another.
Please advise any sort of starting points. to quote the CEO from the movie "Margin Call"
"Please, speak as you might to a young child, or a golden retriever"