STM32F103 BLUEPILL IS NOT DETECTING
Dear STM32 Bluepill Community,
I recently acquired an STM32 Bluepill development board and have been attempting to establish a communication link with my computer via the USB interface. Unfortunately, my computer is not recognizing the COM port associated with the STM32 Bluepill.
Here are the steps I've taken so far to troubleshoot the issue:
Checked the USB Cable and Connection: I have verified that I am using a functional USB cable and ensured that it is properly connected to both the STM32 Bluepill and my computer.
Installed the STM32 Virtual COM Port Driver: Following the guidelines provided by STMicroelectronics, I downloaded and installed the STM32 Virtual COM Port Driver corresponding to my operating system (Windows) and architecture (64-bit).
Checked the Device Manager (Windows): After installing the USB driver, I opened the Device Manager on my Windows computer to verify if the STM32 COM port is detected, but unfortunately, it is not appearing in the list of Ports (COM & LPT).
Despite these efforts, I am still unable to establish a connection between my STM32 Bluepill and my computer. I am seeking assistance from the community to help me identify the potential causes of this issue and find a suitable solution.
Has anyone encountered a similar problem with the STM32 Bluepill not being recognized as a COM port on Windows? If so, how did you resolve it? Are there any additional troubleshooting steps that I should follow to ensure successful communication between the STM32 Bluepill and my computer?
Note: on windows 11 OS
Your guidance and expertise in this matter would be greatly appreciated.