STM32F103 CAN filter range of ID's
Hello, I have a set of extended CAN ID's I need to pas the bxCAN filter. I looked at some examples where one ID is passed the filter, but could not figure out how to allow a set of ID's. If my understanding is correct the mask is used to determine which bits of the ID are important. How can I configure the filter so that I can pass a set of different ID's?
These are the ID's:
// 0x0CF00400
// 0x0CFD9200
// 0x18FEE500
// 0x18FEEE00
// 0x18FEEF00
// 0x18FEF200
// 0x18FEF700
// 0x18FEFC00
This is what my filter config looks like:
can_fil.FilterBank = 0;
can_fil.FilterMode = CAN_FILTERMODE_IDLIST;
can_fil.FilterFIFOAssignment = CAN_RX_FIFO0;
can_fil.FilterIdHigh = 0;
can_fil.FilterIdLow = 0;
can_fil.FilterMaskIdHigh = 0;
can_fil.FilterMaskIdLow = 0;
can_fil.FilterScale = CAN_FILTERSCALE_32BIT;
can_fil.FilterActivation = ENABLE;
can_fil.SlaveStartFilterBank = 13;