STM32F103 UART and USART clock configuration
I am working on a project that uses STM32F103 and STM32G4 as MCUs. They need to communicate between each other using UART. I am trying to configure STM32F103 UART clocks to match the STM32G4's clocks but I have not been able to figure out where to do that. I found a document that says UART clock is based on HCLK, but is there any prescaler that configures the UART clocks? If not, what is the frequency the UART clocks are based in so I can match it by configuring the STM32G4s clock, instead.
To be more specific, I am using all ports as asynchronous. USART1, USART2, USART3, UART4, and UART5.