STM32F103 usb data loss
I'm trying out a test program to measure data rate between pc and mcu over usb.
I'm using winusb with winusbnet wrapper on pc side and for mcu firmware i followed this github repo
https://github.com/MichaelTien8901/STM32WINUSB
to get it built with winusb support.
On the device I have allocated 1024 byte TX and RX buffers for usb.
And used the same code from the repo
static int8_t CDC_Receive_FS(uint8_t* Buf, uint32_t *Len)
{
/* USER CODE BEGIN 6 */
extern volatile int8_t data_out_flag;
#define RX_DATA_LEN 1024
uint32_t receive_len = *Len;
if ((data_received + receive_len)> RX_DATA_LEN ) {
receive_len = RX_DATA_LEN - data_received;
if ( receive_len != 0 )
memcpy(RxData+data_received, Buf, receive_len);
data_received= RX_DATA_LEN;
} else {
memcpy(RxData+data_received, Buf, receive_len);
data_received += receive_len;
}
data_out_flag = 1;
USBD_CDC_SetRxBuffer(&hUsbDeviceFS, &Buf[0]);
USBD_CDC_ReceivePacket(&hUsbDeviceFS);
return (USBD_OK);
/* USER CODE END 6 */
}
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
if ( data_out_flag ) {
extern int8_t CDC_is_busy(void);
if ( CDC_is_busy()) continue;
data_out_flag = 0;
data_sent = data_received;
memmove( TxData, RxData, data_received );
data_received = 0;
CDC_Transmit_FS( TxData, data_sent );
}
}
/* USER CODE END 3 */
}
int8_t CDC_is_busy(void)
{
USBD_CDC_HandleTypeDef *hcdc = (USBD_CDC_HandleTypeDef*)hUsbDeviceFS.pClassData;
if (hcdc->TxState != 0)
return 1;
else return 0;
}
From my tests on pc software in a loop I make
1. Test1: 5 calls to `writePipe` with 60 bytes each
2. Test2: 5 calls to `writePipe` with 120 bytes each
3. Test3: 5 calls to `writePipe` with 240 bytes each
Each of this is a seperate test...
I notice with a USB analyzer that I only get 3 calls of data back from device... and the last call is much bigger than the first 2.
Even if i increase the 5 calls to 10 calls on pc side i only get 3 back...and I see typically the last result i get back is truncated and the data is limited to 1024 byte similar to the buffer that is allocated on the device.
so the first response and second response from the device is typically around 64 bytes and the third one is a much bigger packet as if its trying to stuff everything else in that response..
I'm probably thinking there is something wrong going on in my device code... and its unable to process the requests at a fast enough rate.
Any ideas and clues on this would be really helpful.