Skip to main content
This topic has been closed for replies.
Best answer by liaifat85

Using a resonator with 33pF instead of the recommended 20pF might slightly shift the resonant frequency and increase startup time. This effect is usually small but may vary based on the sensitivity of your application.

3 replies

Technical Moderator
November 3, 2024

IMG_0283.jpeg

Dear @pilot ,

 

Resonators are a bit different from Crystals as they have their built-in CL1 and CL2, this murata resonator has 33pF C1/C2 which is different from Crystal CL . In general CL1/CL2 value are in range of twice for crystal for the value of CL  - Stray /Parasitic .

Here this resonator is fully compatible with STM32F1 series . You can use no worries.

IMG_0282.jpeg

You can also refer to our Application Note :

https://www.st.com/resource/en/application_note/an2867-guidelines-for-oscillator-design-on-stm8afals-and-stm32-mcusmpus-stmicroelectronics.pdf#

I’m interesting to know the end application usage, this resonator has 8MHz ( -/+ 0.5%) you can use built-in HSI . 

Hope it helps ,

STOne-32.

 

liaifat85Answer
Visitor II
November 3, 2024

Using a resonator with 33pF instead of the recommended 20pF might slightly shift the resonant frequency and increase startup time. This effect is usually small but may vary based on the sensitivity of your application.

pilotAuthor
Graduate II
November 3, 2024

Thank you, will test. Startup time is not an issue, nor is the frequency precision very important.

pilotAuthor
Graduate II
November 3, 2024

@STOne-32  The application consists basically of the device doing AD  , communicating on I2C  (100khz) and serial(USB)  I have simply no low frequency oscillator as there is no clock/sleep.

I must say I did not even look at the option to use HSI.

The device will see temperatures within -20+40°C 

 

Graduate II
November 3, 2024

For USB you want HSE

Also HSI+PLL gets you to 64 MHz on the F1

pilotAuthor
Graduate II
November 3, 2024

Ah, thank you - I knew about 64Mhz, but that is plenty enough, but the USB was a good point