Skip to main content
Explorer
June 30, 2024
Solved

stm32f103vet6 no osc no cap Swd download ok

  • June 30, 2024
  • 1 reply
  • 916 views

no osc no resist no osc but it run and download with swd light led pb12 ,but when fixed pin anybody know 

67C5C88B-4C82-4A2F-A99C-F5919B6B3DFC.jpeg

1496A3E0-41E3-4B6D-8C67-F9462D889761.jpeg

  • v2.9.0 
     -------------------------------------------------------------------
    
    ST-LINK SN : 16004A002933353739303541
    ST-LINK FW : V2J38S7
    Board : --
    Voltage : 3.17V
    SWD freq : 4000 KHz
    Connect mode: Under Reset
    Reset mode : Hardware reset
    Device ID : 0x414
    Revision ID : Rev X
    Device name : STM32F101/F103 High-density
    Flash size : 512 KBytes
    Device type : MCU
    Device CPU : Cortex-M3
    BL Version : --
    
    
    
    Memory Programming ...
    Opening and parsing file: BlinkSTM32FC8.ino.bin
     File : BlinkSTM32FC8.ino.bin
     Size : 12944 Bytes
     Address : 0x08000000 
    
    
    Erasing memory corresponding to segment 0:
    Erasing internal memory sectors [0 6]
    Download in Progress:
    
    
    File download complete
    Time elapsed during download operation: 00:00:00.774
    
    RUNNING Program ... 
     Address: : 0x8000000
    Application is running, Please Hold on...
    Start operation achieved successfully
    This topic has been closed for replies.
    Best answer by STOne-32

    Dear @st128 ,

     

    Welcome in STCommunity !  and glad to see it is working and so robust - However at real application you should follow minimum Hardware and passive components as this Application Note 

    Getting started with STM32F10xxx hardware development - undefined

    Hope it helps you.

    STOne-32.

    1 reply

    STOne-32Answer
    Technical Moderator
    June 30, 2024

    Dear @st128 ,

     

    Welcome in STCommunity !  and glad to see it is working and so robust - However at real application you should follow minimum Hardware and passive components as this Application Note 

    Getting started with STM32F10xxx hardware development - undefined

    Hope it helps you.

    STOne-32.

    st128Author
    Explorer
    July 1, 2024

    o,thank you