Solved
Stm32f105 don't enter dfu mode
Posted on November 05, 2012 at 11:29
Hello,
I designed a board which contains stm32f105 microcontroller, and i want to use DFU as bootloader in order to download my program to the micro controller through usb port. I put BOOT0 =1, and BOOT1=0 PA10=PD6=PB5=0 then i powered the circuit and connected it to usb port of my pc which runs windows xp. But the pc didn't recognise a new device. These are the processor data: STM32F105 VCT6 Z 990TD 93 MYS 99 045 First question: Why the pc didn't recognize a new device? Second question: the date code is 045 what year does this mean? Regards, Hisham