STM32F302: I2C slave transmitter nacking when no data is to be sent
Hello,
I'd like to have this feature implemented: if no data is to be sent, the I2C peripheral (in the slave mode) should not perform an ACK in case of an address match.
Of course, this wouldn't have to be an issue, if, for example, no data is ready, the interrupt routine would respond with a "no data" answer, for example sending 0xFF. However, I'm working with a codebase, where this behavior is not desired.
I was thinking about configuring the I2C peripheral in this way:
setting the SBC bit to 1 - if NBYTES=0 and the slave is addressed to send data to the master, what happens in this case?
Thank you in advance.