STM32F302R8 an error occurs after burning the hex file
I always get an error after burning the hex file to STM32F302R8. The burning is completed through STM32 ST-LINK Utility. Below is the error log.
16:05:15 : ST-LINK SN : 0664FF515570514867174448
16:05:15 : V2J33M25
16:05:15 : Connected via SWD.
16:05:15 : SWD Frequency = 4,0 MHz.
16:05:15 : Connection mode : Connect Under Reset.
16:05:15 : Debug in Low Power mode enabled.
16:05:16 : Device ID:0x439
16:05:16 : Device flash Size : 64KBytes
16:05:16 : Device family :STM32F301x4-x6-x8/F302x4-x6-x8/F318xx
16:05:23 : Memory programmed in 1s and 594ms.
16:05:23 : Disconnected from device.
16:05:23 : Connection to device is lost: check power supply and debug connection.
16:05:23 : If the target is in low power mode, please enable "Debug in Low Power mode" option from Target->settings menu.