Skip to main content
Explorer
January 23, 2024
Question

STM32f303

  • January 23, 2024
  • 2 replies
  • 1022 views

IMG-20240123-WA0006.jpg

In 50% of the PCB s where the STM32f303 (with the Y revision ) was in we were unable to code a program , as well as that problem we had some difficulties with the UART It won’t connect to the laptop, it says that the device is unrecognizable and that it does recognize the COM port.
In the picture down below you can see the unstable signals (they are marked)

    This topic has been closed for replies.

    2 replies

    Technical Moderator
    January 23, 2024

    Welcome @DianaSok, to the community!

    What exactly do you mean by "unable to code a program", i.e. what do you want to programme and what errors occur?

    Which program on your laptop returns the error that the device is not recognisable?

    What do you mean by unstable signals, or what signals do you expect?

    Regards
    /Peter

    Graduate II
    January 23, 2024

    Sorry, your presentation of the problem isn't terribly helpful.

    We're Non-Y parts less problematic? Did prior batches of boards work?

    What does "unable to code a program" mean? That the download failed? That the verify failed? That the code failed to run at startup? You're going to have to be a lot more specific and detailed in your observations..

    Add some output telemetry for Error_Handler, HardFault_Handler and clock speeds and status.