Skip to main content
Visitor II
July 22, 2025
Question

STM32F373CCT6 SDADC initializing problem

  • July 22, 2025
  • 1 reply
  • 249 views

Hi, I'm trying to initialize SDADC of my STM32F373CCT6 chip based on the Standard Peripherial Library. The program can be compiled with no errors but doesn't work after I uploaded it to the chip. I used a LED program to test it and found that the initializing function got stucked at the statement of waiting for calibration to complete. I used a self designed board. The intializing function and the main function of my program, as well as the schematic diagram of my board is attached. I'm a STM32 beginner and haved been troubled by this issue for days, I sincerely hope to get your help. Thank you so much!

    This topic has been closed for replies.

    1 reply

    Super User
    July 22, 2025

    If you're a beginner, I recommend using HAL instead of the SPL. It is better in every way. CubeMX will generate the initialization code for you.