STM32F4 Discovery 1-2% Accuracy ADC
I am just now moving over from ESP32 to STM32 Discovery. One of the features that I like about the STM32 is that there are 3 ADC and several accessible channels.
In my previous design on the ESP32 I used external ADCs and communicated with them using SPI. I'm hoping I can cut out the external ADCs.
In the STM32F4 Discovery schematic it shows how the VDDA and VREF+ pins are connected so no external (highly accurate) reference voltage can be applied without cutting traces (which is not preferred).
Also I have found recommendations for reading the VREF+ voltage level with software and comparing it to the reading from the ADC. This makes sense in theory and since I'm not concerned about sample rate at this point I think it is a viable option. And if there was noise on VREF+ line or the input I can take an average of many samples.
I'll need to try it out for myself but wondering if anyone has experience and can recommend which method (or a different method) would work best for accurate ADCs readings. Ideally I can get .1-.2% accuracy from the ADC which is right around what the sum of the errors ADC errors, but is it too much to ask to actually achieve this accuracy? If not I will have to stick with external ADCs.