STM32F4 in hardfault caused by CAN
Hello everyone,
I am using an STM32F405 for a communication over can. It is receiving the messages on CAN1 and CAN2. For drivers I use STM32_HAL. My initialization procedure goes the following way:
- Init clocks
- Init GPIOs
- Init CAN
- Init CAN peripheral
- Init filters
- Activate notification(CAN_IT_RX_FIFO0_MSG_PENDING, CAN_IT_RX_FIFO0_OVERRUN)
- HAL_CAN_Start
I repeat this for CAN1 and CAN2.
The code is fine, when the can messages start arriving some time after the CAN peripheral is initialized, but if it arrives immediately then microcontroller ends in a HardFault.
In the production environment there are two devices on each bus: microcontroller and BMS. In this setup the HardFault occurs regularily, as microcontroller doesn't ACK the CAN frame which then BMS retries immediately. If I add a PCAN, which ACKs the messages the BMS sends Microcontroller works fine, but this is not the situation we have in production.
I've found the workaround: call HAL_CAN_Start 5 seconds later, then there is no HardFault, but I would like to understand why is this happening if I call it immediately. Is there some time that should be left for the peripheral to 'settle in' after the Init, or did I do something else wrong?