STM32F401RE Pushbutton interrupt
So here's the code ; The issue with it is that whenever I press the button, weird things occur, such as my output resetting completely-going to the maximum, at my output I have a variable PWM signal
void PB_Init(void){
RCC->AHB1ENR |= RCC_AHB1ENR_GPIOCEN;
GPIOC->MODER |= ( 0x0 << GPIO_MODER_MODE13_Pos);
GPIOC->PUPDR |= ( 0x1 << GPIO_PUPDR_PUPD13_Pos);
}
void EXTI15_10_Init(void){
PB_Init(); // Initialize PC13 as input.
RCC->APB2ENR |= (1<<14); // Enable System configuration controller
SYSCFG->EXTICR[3] &= ~(1<<7); // Select Port C as source, EXTIx = 0b0010
SYSCFG->EXTICR[3] &= ~(1<<6); // Select Port C as source, EXTIx = 0b0010
SYSCFG->EXTICR[3] |= (1<<5); // Select Port C as source, EXTIx = 0b0010
SYSCFG->EXTICR[3] &= ~(1<<4); // Select Port C as source, EXTIx = 0b0010
EXTI->IMR |= (1<<13); // Disable interrupt request mask on EXTI line 13
EXTI->FTSR |= (1<<13); // Enable EXTI on Falling edge
EXTI->RTSR &= ~(1<<13); // Disable EXTI on Rising edge
RCC->APB2ENR &= ~(1<<14); // Disable System configuration controller
}
volatile bool flag=0;
void EXTI15_10_IRQHandler(void){
if(flag==0){
TIM2->CR1|=TIM_CR1_CEN;
flag=!flag;
EXTI->PR |= (1<<13); // Clear PR to re-enable EXTI interrupt
}else{
TIM2->CR1&=~TIM_CR1_CEN;
flag=!flag;
EXTI->PR |= (1<<13); // Clear PR to re-enable EXTI interrupt
}
}
void Interrupt_Init(void){
EXTI15_10_Init(); // Step 1, this is defined elsewhere
NVIC->IP[EXTI15_10_IRQn] = (1 << 4); // Step 3: Set priority to 1
NVIC->ISER[40 >> 5] |= (1 << (40 % 32)); // Step 4: Enable interrupt
}
, can anyone point me in the right direction?