STM32F405 Can not connect to target
Hello All, I Hope you are well.
I am facing a problem that I spent A LOT of time on. I designed a custom board featuring the STM32F405RGT6 but i cannot connect to it at all.. I will attach the schematic and the board's pictures below. (The schematic is a PDF where I attached the sheet of the MCU's circuitry only there are other sheets for other parts of the board)
Things to mention:
1- I've assembled the board myself (But i checked the connectivity and voltages on the necessary nodes by a multimeter and i tested on the chip's pins not on the PCB pads and got the following:
-VDD on all VDD pins are 3.31V (measured directly on the pins)
-VDDA is also supplied by the same source with around 3.31V (measured directly on the pins)
-Vcap1 and Vcap2 are both 1.26V (measured on the the two Caps of 2u2 value)
-Reset Pin is 3.31V
)
2- I got suspicious about the SWD pinout that i did so i used an adapter and a Nucleo board's ST-Link to connect to my board where I measured the resistance between the SWD Pins and the Nucleo board and all are connected with reasonable resistance (Under 10 Ohms) (I got so desperate of the cause that I replaced the termination resistors of 49R9 with 0Ohms ones)
3- I got in both modes of Boot0 being Low and High. (Boot1 is floating would that cause the lack of connectivity?)
Am I missing something?!
Any kind of help would be much much appreciate. Thank you in Advance.