STM32F405RGT6 TIM Output Signal Becomes Unstable at 60°C While Room Temperature is Normal
Tests Performed and Results:
1.A DC regulated power supply was used to provide 14V to the board directly. At room temperature, the CPU's TIM pin output is normal. However, at high temperatures, the output waveform becomes intermittent.
2.The on-board 3.3V and 5V power supplies remain stable and within specification at all times.
3.The external crystal oscillator connected to the microcontroller maintains a stable waveform under all temperature conditions.
4.The same issue occurs even after replacing the CPU with one from a previous production batch: the TIM pin output is normal at room temperature but becomes intermittent at high temperatures.
5.This TIM pin is used to simulate a frequency signal. When the output becomes intermittent, the total output duration becomes longer. The firmware uses a pulse count to determine when to stop the output, so it appears the missing pulses (due to missed interrupts) cause the output to last longer than expected.
Questions:
Given the above results, what should I do next?
Should I contact ST technical support, and if so, how can I submit a support ticket correctly?