Skip to main content
Explorer II
April 27, 2024
Question

STM32F407-BareMetal Clock Setting not working

  • April 27, 2024
  • 0 replies
  • 558 views

Hi all, I tried to configure the clock to run at 32MHz and I was using Systick to toggle the LED every 1 Sec by configuring the Systick reload value by 32Mhz -1. But, Somehow toggling is not happening for exactly 1 sec, and also used a logic analyzer to check the period and it was not 1 sec. Somehow, I am not able to figure out the problem.
I selected HSE(8MHz)  and PLL as a System clock. PLLM = 2,PLLN=16,PLLP=2. AHB prescaler as 1.

RCC.h

#include <stdint.h>

 

#ifndef RCC_H_

#define RCC_H_

 

#define RCC_BASE_ADDR 0x40023800 /* Base Addr of RCC */

#define FLASH_INTR 0x40023C00 /* Base of Flash Interface Register */

 

#define RCC_CR *(volatile uint32_t*)(RCC_BASE_ADDR + 0x00)

#define RCC_PLLCFGR *(volatile uint32_t*)(RCC_BASE_ADDR + 0x04)

#define RCC_CFGR *(volatile uint32_t*)(RCC_BASE_ADDR + 0x08)

#define RCC_APB1RSTR *(volatile uint32_t*)(RCC_BASE_ADDR + 0x20)

 

#define FLASH_ACR *(volatile uint32_t*)(FLASH_INTR + 0x00)

 

void clock_init();

void clock_init1();

 

#endif /* RCC_H_ */

RCC.c

#include "rcc.h"

void clock_init()
{

        FLASH_ACR |=(1<<0); /* 1 wait states */
        RCC_CR |= (1<<16); /* HSE oscillator is ON */

        while(!(RCC_CR & (1<<17))); /* wait till HSE oscillator is ready */

        RCC_PLLCFGR |= (2<<0); /* PPLM is selected */
        RCC_PLLCFGR |= (16<<6); /* PPLN is selected */
        RCC_PLLCFGR |= (0<<16); /* PPLP is selected */
        RCC_PLLCFGR |= (2<<24); /* PPLQ is selected */
        RCC_PLLCFGR |= (1<<22);  /* HSE is selected as SRC for PLL */

        RCC_CFGR |= (0<<4); /* AHB Pre-scaler */
        RCC_CFGR |= (0<<10); /* APB1 Pre-sclaer */
        RCC_CFGR |= (0<<13); /* APB2 Pre-sclaer */

        RCC_CR |= (1<<24); /* PLL is enabled */

        while(!(RCC_CR & (1<<25))); /* wait till PLL oscillator is ready */

        RCC_CFGR |= (2<<0);  /* PLL selected as system clock */

        while(!(RCC_CFGR & (2<<2))); /* wait till PLL to be clock */

}

Main.c
#include <stdint.h>
#include "GPIO.h"
#include "rcc.h"

void delay1(void);
void Systick_Init(void);

#define SYST_CSR    *(volatile uint32_t*)(0xE000E010) /* Systick controller register */
#define SYST_RVR    *(volatile uint32_t*)(0xE000E014) /* Systick Reload Register */

int main(void)
{
    clock_init();
    GPIOA_Init();
    Systick_Init();
}

void Systick_Init()
{
    /* SysTick Reload value = System clock(Hz) x Delay Desired(s) */
    /*
    Reload value = ((Clock_Speed(Hz)/Desired_Tick(Hz))-1))
    Here 1sec is required to generate systick interrupt, so the Desired Tick is 1Hz(1Sec)
    and clock speed is 16MHz
    */
    SYST_RVR =  32000000-1; /* Reload value */
    SYST_CSR |= 0x07UL; /* Enable counter, systick interrupt, clk source as processor clk */
}

void SysTick_Handler()
{
    GPIO_ODR ^= (1<<0);
}

 clock_systick_Led.png

 

    This topic has been closed for replies.