STM32F407 Dual CAN - first CAN instance both tx rx works, second CAN instance only tx works, receive does not
Moved from this post.
Hi @mƎALLEm,
I am facing the same issue with STM32F407. Whichever CAN is master in filter configuration is working, the other one is not.
void can_init() {
CAN_FilterTypeDef sFilterConfig1;
sFilterConfig1.FilterBank = 0;
sFilterConfig1.FilterMode = CAN_FILTERMODE_IDMASK;
sFilterConfig1.FilterScale = CAN_FILTERSCALE_32BIT;
sFilterConfig1.FilterIdHigh = 0x0000;
sFilterConfig1.FilterIdLow = 0x0000;
sFilterConfig1.FilterMaskIdHigh = 0x0000;
sFilterConfig1.FilterMaskIdLow = 0x0000;
sFilterConfig1.FilterFIFOAssignment = CAN_FILTER_FIFO1;
sFilterConfig1.FilterActivation = ENABLE;
sFilterConfig1.SlaveStartFilterBank = 14;
if (HAL_CAN_ConfigFilter(&hcan1, &sFilterConfig1) != HAL_OK) {
Error_Handler();
}
CAN_FilterTypeDef sFilterConfig2;
sFilterConfig2.FilterBank = 14;
sFilterConfig2.FilterMode = CAN_FILTERMODE_IDMASK;
sFilterConfig2.FilterScale = CAN_FILTERSCALE_32BIT;
sFilterConfig2.FilterIdHigh = 0x0000;
sFilterConfig2.FilterIdLow = 0x0000;
sFilterConfig2.FilterMaskIdHigh = 0x0000;
sFilterConfig2.FilterMaskIdLow = 0x0000;
sFilterConfig2.FilterFIFOAssignment = CAN_FILTER_FIFO0;
sFilterConfig2.FilterActivation = ENABLE;
if (HAL_CAN_ConfigFilter(&hcan1, &sFilterConfig2) != HAL_OK) {
Error_Handler();
}
// Start both CAN interfaces
if (HAL_CAN_Start(&hcan1) != HAL_OK) {
Error_Handler();
}
if (HAL_CAN_Start(&hcan2) != HAL_OK) {
Error_Handler();
}
// Activate notifications for both CAN interfaces
if (HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO0_MSG_PENDING) != HAL_OK) {
Error_Handler();
}
if (HAL_CAN_ActivateNotification(&hcan2, CAN_IT_RX_FIFO1_MSG_PENDING) != HAL_OK) {
Error_Handler();
}
}
In the above code, CAN1 is configured with a slave filter bank, CAN2 RX and TX are working, CAN1 only TX is working. I ditched the interrupt and tried with polling also. Same result.
In the below code, CAN2 is configured with slave filter bank, CAN1 RX and TX are working, CAN2 only TX is working. I switched between internal as well as external clock and tried polling.
void can_init() {
CAN_FilterTypeDef sFilterConfig1;
sFilterConfig1.FilterBank = 0;
sFilterConfig1.FilterMode = CAN_FILTERMODE_IDMASK;
sFilterConfig1.FilterScale = CAN_FILTERSCALE_32BIT;
sFilterConfig1.FilterIdHigh = 0x0000;
sFilterConfig1.FilterIdLow = 0x0000;
sFilterConfig1.FilterMaskIdHigh = 0x0000;
sFilterConfig1.FilterMaskIdLow = 0x0000;
sFilterConfig1.FilterFIFOAssignment = CAN_FILTER_FIFO0;
sFilterConfig1.FilterActivation = ENABLE;
sFilterConfig1.SlaveStartFilterBank = 14;
if (HAL_CAN_ConfigFilter(&hcan1, &sFilterConfig1) != HAL_OK) {
Error_Handler();
}
CAN_FilterTypeDef sFilterConfig2;
sFilterConfig2.FilterBank = 14;
sFilterConfig2.FilterMode = CAN_FILTERMODE_IDMASK;
sFilterConfig2.FilterScale = CAN_FILTERSCALE_32BIT;
sFilterConfig2.FilterIdHigh = 0x0000;
sFilterConfig2.FilterIdLow = 0x0000;
sFilterConfig2.FilterMaskIdHigh = 0x0000;
sFilterConfig2.FilterMaskIdLow = 0x0000;
sFilterConfig2.FilterFIFOAssignment = CAN_FILTER_FIFO1;
sFilterConfig2.FilterActivation = ENABLE;
if (HAL_CAN_ConfigFilter(&hcan1, &sFilterConfig2) != HAL_OK) {
Error_Handler();
}
// Start both CAN interfaces
if (HAL_CAN_Start(&hcan1) != HAL_OK) {
Error_Handler();
}
if (HAL_CAN_Start(&hcan2) != HAL_OK) {
Error_Handler();
}
// Activate notifications for both CAN interfaces
if (HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO0_MSG_PENDING) != HAL_OK) {
Error_Handler();
}
if (HAL_CAN_ActivateNotification(&hcan2, CAN_IT_RX_FIFO1_MSG_PENDING) != HAL_OK) {
Error_Handler();
}
}
I even tried configuring `HAL_CAN_ConfigFilter` both using hcan1, both using hcan2, and tried putting seperate handles in seperate CANs. Anyway, only one CAN is working at a time, whichever is made the master.