STM32F407 MCU Maximum Voltage Input
Hi All
Maximum input voltage for this series of MCU per Table II of the datasheet is specified to be 4.0 VDC for all pins other than five-volt tolerant. Table 12 specifies the maximum injected current for all pins other than five-volt tolerant to be +/- 5 mA.
Given the above specifications would it be permissible to exceed the maximum input voltage if the injected current is limited to lets say 0.1 mA by a resistor in series with the non five-volt tolerant I/O pin? If not what would be the reason?
Regards
ik