STM32F407 pulls up pins when debugging
Hello people, i am making a project using STM32F407VG and i am using a timer that drives a laser. The problem is, when debugging STM is probably pulling couple of its pins to High state before i start F8 (between pressing the 'Debug' button and F8 to stop the program waiting at HAL_Init() function after i run the code it switches back to LOW state ) and messes up with my laser circuit. I want to know which pins go to High state and why, and see if i can control it i really have to deny it pulling to high state. Thanks for the help. Have a great day !