Skip to main content
Visitor II
June 24, 2024
Solved

STM32F407 PWM output not stable

  • June 24, 2024
  • 1 reply
  • 914 views

I am trying to set up PWM on Channel 1, 2, 3 of TIM3. At first I set up only Channel 1 and the output voltage of PWM is 2.8V. But after I set up the other two channels, the output voltage of Channel 1 & 3 gets to 3.6V, while that of Channel 2 is still 2.8V. Here is the GPIO and TIM settings of TIM and PWM:

void MX_GPIO_Init(void)

{

GPIO_InitTypeDef GPIO_InitStruct = {0};

/* GPIO Ports Clock Enable */

__HAL_RCC_GPIOF_CLK_ENABLE();

__HAL_RCC_GPIOH_CLK_ENABLE();

__HAL_RCC_GPIOA_CLK_ENABLE();

__HAL_RCC_GPIOB_CLK_ENABLE();

/*Configure GPIO pin Output Level */

// HAL_GPIO_WritePin(GPIOF, GPIO_PIN_6|GPIO_PIN_7|GPIO_PIN_8, GPIO_PIN_RESET);

/*Configure GPIO pins : PF6 PF7 PF8 */

GPIO_InitStruct.Pin = GPIO_PIN_6|GPIO_PIN_7|GPIO_PIN_8;

GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;

GPIO_InitStruct.Pull = GPIO_NOPULL;

GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;

HAL_GPIO_Init(GPIOF, &GPIO_InitStruct);

/*Configure GPIO pin : PA6 PA7 */

GPIO_InitStruct.Pin = GPIO_PIN_6|GPIO_PIN_7;

GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

GPIO_InitStruct.Pull = GPIO_NOPULL;

GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;

GPIO_InitStruct.Alternate = GPIO_AF2_TIM3;

HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

/*Configure GPIO pin : PB0 */

GPIO_InitStruct.Pin = GPIO_PIN_0;

GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

GPIO_InitStruct.Pull = GPIO_NOPULL;

GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;

GPIO_InitStruct.Alternate = GPIO_AF2_TIM3;

HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

}
TIM_HandleTypeDef htim3;
static void TIM_Mode_Config() {

TIM_OC_InitTypeDef sConfigOC;

ADV_TIM_CLK_ENABLE();

// Set TIM3 for all channels.

htim3.Instance = ADV_TIM;

// TIM3 clock freq = 84MHz

// TIM3 actual freq = 84MHz / 84 = 1MHz

htim3.Init.Prescaler = ADV_TIM_PRESCALER - 1;

// PWM freq = 1MHz / 1000 = 1kHz

htim3.Init.Period = ADV_TIM_PERIOD - 1;

htim3.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;

htim3.Init.CounterMode = TIM_COUNTERMODE_UP;

htim3.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE;

HAL_TIM_Base_Init(&htim3);

HAL_TIM_PWM_Init(&htim3);

// Set PWM

sConfigOC.OCMode = TIM_OCMODE_PWM1;

// Duty = 50%

sConfigOC.Pulse = ADV_TIM_DEFAULT_PULSE;

sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;

sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;

HAL_TIM_PWM_ConfigChannel(&htim3, &sConfigOC, TIM_CHANNEL_1);

HAL_TIM_PWM_ConfigChannel(&htim3, &sConfigOC, TIM_CHANNEL_2);

HAL_TIM_PWM_ConfigChannel(&htim3, &sConfigOC, TIM_CHANNEL_3);

HAL_TIM_PWM_Start(&htim3, TIM_CHANNEL_1);

HAL_TIM_PWM_Start(&htim3, TIM_CHANNEL_2);

HAL_TIM_PWM_Start(&htim3, TIM_CHANNEL_3);

}

Any help will be highly appreciated. Thank you all.

    This topic has been closed for replies.
    Best answer by Sarra.S

    Hello @LittleYe233, sorry for the delayed answer, 

    Your code seems ok, is it a custom board? maybe it's a hardware connections issue 

    1 reply

    Sarra.SAnswer
    ST Employee
    August 1, 2024

    Hello @LittleYe233, sorry for the delayed answer, 

    Your code seems ok, is it a custom board? maybe it's a hardware connections issue 

    Visitor II
    August 28, 2024

    Thank you. It is a custom board indeed. I will try to find out what the hardware issue is.