STM32f407 Triple regular simultaneously mode only: no output in ADC_CDR register
I'm trying to acquire data from 3 sensor simultaneously using Triple Mode. Im using TIM 2 TRGO as a trigger for starting ADC. my data are getting correctly generated in the respective DR registers of ADCs but not in Common register ADC->CDR where it is supposed to have the data
void adc_init(void){
// Enable clock
RCC -> AHB1ENR |= (1U << 0); //Clock For GPIOA
RCC -> AHB1ENR |= (1U << 22); //Clock for DMA2
RCC -> APB2ENR |= (1U << 8); //Clock for ADC1
RCC -> APB2ENR |= (1U << 9); //Clock for ADC2
RCC -> APB2ENR |= (1U << 10); //Clock for ADC3
//Config GPIO
GPIOA -> MODER |= (1U << 2) | (1U <<3); //Analog mode PA1
GPIOA -> MODER |= (1U << 4) | (1U <<5); //Analog mode PA2
GPIOA -> MODER |= (1U << 6) | (1U << 7); //Analog mode PA3
//Triple Mode ADC1, ADC2, ADC3
ADC->CCR |= (0x0016); // Triple Regular Simultaneous Mode
//ADC1 Config
//Select channel
ADC1 -> SQR3 &= ~( (1U << 1) | (1U << 2) | (1U << 3) | (1U << 4));
ADC1 -> SQR3 |= (1U << 0);
ADC1->SMPR2 |= (1U << 0);
ADC1 -> CR2 |= (1U << 28); //Enable External trigger
ADC1 -> CR2 &= ~(1U << 29);
ADC1 -> CR2 |= ( 1U << 28 ); // Enable external trigger on rising edge for ADC1
ADC1 -> CR2 |= ( 1U << 29 );
ADC1 -> CR2 &= ~(1U << 24); // Select TIM2 TRGO event for external trigger
ADC1 -> CR2 |= (1U << 25);
ADC1 -> CR2 |= (1U << 26);
ADC1 -> CR2 &= ~(1U << 27);
ADC1 -> CR2 |= (1U << 0);
// ADC1 -> CR2 |= (1U << | (1U << 9); // Select to use DMA
//ADC2 Config
//Select channel
ADC2 -> SQR3 &= ~( (1U << 0) | (1U << 2) | (1U << 3) | (1U << 4));
ADC2 -> SQR3 |= (1U << 1);
ADC2->SMPR2 |= (1U << 0);
ADC2 -> CR2 |= (1U << 0);
//ADC3 Config
ADC3 -> SQR3 &= ~( (1U << 2) | (1U << 3) | (1U << 4));
ADC3 -> SQR3 |= (1U << 0) | (1U << 1);
ADC2->SMPR2 |= (1U << 0);
ADC3 -> CR2 |= (1U << 0);
/* CONFIG TIMER FOR TRIGGER */
RCC -> APB1ENR |= ( 1U << 0); // Enable clock for TIM2
TIM2 -> PSC = (8400 - 1); // Set prescaler for 10000Hz timer frequency
TIM2 -> ARR = (1000-1); // Set auto reload value
TIM2 -> CR2 &= ~(( 1U << 4) | ( 1U << 6)); // Select update event for TRGO
TIM2 -> CR2 |= ( 1U << 5);
}
void adc_start(void){
TIM2 -> CR1 |= ( 1U << 0); // Enable TIM2
}