STM32F407: UART transmit stopped when USB is receiving
I simplified the code belows ;
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USB_DEVICE_Init();
MX_USART2_UART_Init();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
HAL_Delay(1000);
// CDC_Transmit_FS(buff , sizeof(buff));
// if (user_inp[0]=='x'){
// CDC_Transmit_FS(buff , sizeof(buff));}
//
// else{
// CDC_Transmit_FS(user_inp,2);}
//readbuff[0] = user_inp[0];
//readbuff[1] = user_inp[1];
// if (user_inp[0]=='x'){
// HAL_UART_Transmit(&huart2, readbuff,sizeof(readbuff),0xff);}
//
//
// else{ HAL_UART_Transmit(&huart2, buff,sizeof(buff),0xff);}
HAL_UART_Transmit(&huart2, buff,sizeof(buff),0xff);
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
the only code is uart_trans,i open two windows for uart(ttl to usb) and usb com.after i reset ,the uart trans data per second.when i send data to the usb,the uart trans stops suddenly.is there something interrupt uart?