Skip to main content
Graduate II
August 13, 2025
Question

STM32F407 USB Serial Device class testing

  • August 13, 2025
  • 1 reply
  • 398 views

Hey, I have a custom STM32F407 based board with USB.
USB_P is connected to PA12

USB_N is connected to PA11

LPetr1_0-1755067803007.png



In the STM32CubeMX I have configured USB Device and in the middleclass I have enabled Communication Device Class (Virtual Port Com) for the Class for FS IP.

My main.c code:

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2025 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "usb_device.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include "printf.h"
#include "scpi/scpi.h"
#include "scpi-def.h"
#include "usbd_cdc_if.h"
/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
UART_HandleTypeDef huart4;

/* USER CODE BEGIN PV */
extern uint8_t UserRxBufferFS[APP_RX_DATA_SIZE];
extern uint8_t UserTxBufferFS[APP_TX_DATA_SIZE];
extern uint8_t is_new_data_ready;
extern uint16_t new_data_length;
/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_UART4_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_UART4_Init();
 MX_USB_DEVICE_Init();
 /* USER CODE BEGIN 2 */
 SCPI_Init(&scpi_context,
 scpi_commands,
 &scpi_interface,
 scpi_units_def,
 SCPI_IDN1, SCPI_IDN2, SCPI_IDN3, SCPI_IDN4,
 scpi_input_buffer, SCPI_INPUT_BUFFER_LENGTH,
 scpi_error_queue_data, SCPI_ERROR_QUEUE_SIZE);
 printf("Hello from ST32F407 \n");

 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
	 if (is_new_data_ready) {
	 SCPI_Input(&scpi_context, UserRxBufferFS, new_data_length);
	 is_new_data_ready = 0;
	 }
 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure the main internal regulator output voltage
 */
 __HAL_RCC_PWR_CLK_ENABLE();
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_HSE;
 RCC_OscInitStruct.HSEState = RCC_HSE_ON;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
 RCC_OscInitStruct.PLL.PLLM = 4;
 RCC_OscInitStruct.PLL.PLLN = 72;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
 RCC_OscInitStruct.PLL.PLLQ = 3;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief UART4 Initialization Function
 * None
 * @retval None
 */
static void MX_UART4_Init(void)
{

 /* USER CODE BEGIN UART4_Init 0 */

 /* USER CODE END UART4_Init 0 */

 /* USER CODE BEGIN UART4_Init 1 */

 /* USER CODE END UART4_Init 1 */
 huart4.Instance = UART4;
 huart4.Init.BaudRate = 115200;
 huart4.Init.WordLength = UART_WORDLENGTH_8B;
 huart4.Init.StopBits = UART_STOPBITS_1;
 huart4.Init.Parity = UART_PARITY_NONE;
 huart4.Init.Mode = UART_MODE_TX_RX;
 huart4.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 huart4.Init.OverSampling = UART_OVERSAMPLING_16;
 if (HAL_UART_Init(&huart4) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN UART4_Init 2 */

 /* USER CODE END UART4_Init 2 */

}

/**
 * @brief GPIO Initialization Function
 * None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOH_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();

/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * file: pointer to the source file name
 * line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

 For handling USB data, I have ported the code from the github repository:
https://github.com/Jana-Marie/stm32g4xx_usb_cdc
The USB communication seem to work fine - I can send and receive data via the USB Virtual com port:

LPetr1_1-1755067973982.png

 

Since this is my first time dealing with USB, I have decided to hook up my Saleae logic analyzer to usb D+ and D- pins to inspect how it works and what it sends.

This is my Analyzer configuration:

LPetr1_2-1755068060408.png
But I am very confused about USB decode level, what should I choose?

LPetr1_0-1755069170638.png

 

And I notice things I did not expect to see. When I have the virtual com port disabled (not connected), I see the following:

LPetr1_0-1755068761266.png

If I zoom in, I see the following:

LPetr1_1-1755068780625.png

 

 

As soon as I open the com port, I see the following:

LPetr1_2-1755068830697.png

 

If I zoom in, it looks as following:

LPetr1_3-1755068848595.png

 

 

 

 

When I try to send data via com port, I get the expected response:

MEASure:VOLTage:DC:OUTput?
1337
MEASure:VOLTage:DC:OUTput?
1337
MEASure:VOLTage:DC:OUTput?
1337
MEASure:VOLTage:DC:OUTput?
1337
MEASure:VOLTage:DC:OUTput?
1337


But I cannot make anything out from the D- and D+ lines when sending/receiving.


I want to understand whether this behaviour is normal.

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    August 13, 2025

    Hi @LPetr.1 

    It's complicated to follow USB signaling and protocol analysis at the physical layer ! Using USB sniffer or analyzer is way practical to understand USB traffic. You need to Learn USB fundamentals, focus on understanding USB device states, enumeration, endpoints, and class protocols (like CDC for virtual COM ports) before diving into electrical signaling details.

    LPetr.1Author
    Graduate II
    August 13, 2025

    That makes sense, but for the time being, I just need to understand whether that is something I should worry and that indicates some real USB problem or that is normal behaviour for USB?

    I am quite confusef about all those packets coming thriugh for no reason, but at the same time I am happy that I seem to be able to send commands and receive valid responses via the USB cdc virtual port, so that must be a good sign.

     

    Additionally, perhaps you can recommend some USB debugging tools that I can use to further analyze my USB behaviour and additionally perhaps some usb reading material to get me started about this protocol and not overwhelm me with unnecessary complicated information. Anyway, thanks for your response :)