Skip to main content
Super User
June 9, 2025
Solved

STM32F407 VDDA-VREF+ difference

  • June 9, 2025
  • 3 replies
  • 585 views

In the STM32F407 DS, ADC characteristics table has the following footnotes:

waclawekjan_0-1749462029823.png

IMO 2. follows from 3. (which is a more stringent requirement); thus 2. is redundant and confusing.

JW

    This topic has been closed for replies.
    Best answer by mƎALLEm

    Hello,

    Note 2, is related to the power-up phase while note 3 is related to the functional mode when the ADC is running.

    So note 2 will be updated to mention that difference.

    The proposed change:

    2. When VDDA and VREF+ are supplied by independent voltage sources, during power-up phase, it is recommended to maintain the difference between VDDA and VREF+ below 1.8V.

    3 replies

    Technical Moderator
    June 9, 2025

    Hello,

    This will be escalated internally for analysis and fix. Internal ticket number: 211812.

    Thank you.

    mƎALLEmAnswer
    Technical Moderator
    June 17, 2025

    Hello,

    Note 2, is related to the power-up phase while note 3 is related to the functional mode when the ADC is running.

    So note 2 will be updated to mention that difference.

    The proposed change:

    2. When VDDA and VREF+ are supplied by independent voltage sources, during power-up phase, it is recommended to maintain the difference between VDDA and VREF+ below 1.8V.

    Super User
    June 18, 2025

    Thanks for the clarification.

    JW