STM32F411 HSE Ceramic Resonator external resistor value
Hello everyone,
I'm current creating my first STM32 design using STM32F411 and have a need for the USB function on the MCU. The datasheet states that it requires a 48 MHz clock generated by a PLL connected to the HSE oscillator.
And I've currently chosen the CSTNE8M00G520000R0 ceramic resonator by muRata with built in capacitors for HSE.
Now with my understanding of an2867, I need to calculate the external resistor value based on ESR for crystal based designs.
Based on this post, it seems that ceramic resonator require external resistor, too.
However, I couldn't seem to find the ESR or maximum DL value on the webpage or datasheet of the ceramic resonator.
So my question is if I need an external resistor, and if so, what value should be?
Sorry if I'm not clear enough and thanks in advance.