Skip to main content
Visitor II
June 4, 2025
Question

STM32F412ZETx - CAN2 RX FIFO1 Interrupt Not Triggering (Tx Working)

  • June 4, 2025
  • 2 replies
  • 569 views

I'm working with an STM32F412ZETx microcontroller and encountering an issue with the CAN2 peripheral. The transmit (Tx) functionality is working correctly, but the receive (Rx) interrupt via FIFO1 is not triggering at all.

 

CAN2 transmit works fine. I can see messages on the bus. same setup with CAN1 (Rx FIFO0) works fine.

Is there anything specific I need to configure for CAN2 RX interrupts on STM32F412?

Could the filter bank or SlaveStartFilterBank setting be causing this?

Are there known limitations with CAN2 and FIFO1 on this device?

    This topic has been closed for replies.

    2 replies

    Graduate II
    June 11, 2025

    Did you enable the NVIC?

    Technical Moderator
    June 11, 2025

    Hello,

    You have an issue with the filter bank configuration:

     sFilterConfig.FilterBank = 0;
     sFilterConfig.SlaveStartFilterBank = 14;

     FilterBank should be >= SlaveStartFilterBank.

    Refer to this article: STM32 in dual CAN configuration: bxCAN Filter bank explanation and relation with CAN2 Start Bank parameter

    Technical Moderator
    June 11, 2025

    @mƎALLEm wrote:

    Hello,

    You have an issue with the filter bank configuration:

     sFilterConfig.FilterBank = 0;
     sFilterConfig.SlaveStartFilterBank = 14;

     FilterBank should be >= SlaveStartFilterBank.

    Refer to this article: STM32 in dual CAN configuration: bxCAN Filter bank explanation and relation with CAN2 Start Bank parameter


    Sorry what I saw is the code related to CAN1.

    As said by @Karl Yamashita you need to check if you enabled CAN2 NVIC Rx for FIFO1