STM32F427 PWM on 40 pins with DMA and BSRR
Hi,
I need to generate ~8khz PWM on 40 pins with at least 1% resolution. I was thinking about solution using GPIO ports D,G,F and DMA2 streams 1,2, 7 which are all triggered by TIM8 (TIM8_UP, TIM8_CH1, TIM8_CH4/TRIG/COM).
I am worried about the data transfer speed of the DMA. 8khz, with 1% resolution means 0,8Mhz x 3 ports = 2,4Mhz DMA streams. Reffering to documentation it takes about 8 APB clock cycles to process and perform DMA transfer which means that it takes about ~20M clockcycles/sec and APB2 is running currently at 84Mhz. This seems quite a lot and Im worried about saturating the bus.
Can someone correct me please? How big of a problem this could potentially be? How fast i can go with this?
Thank you very much in advance!