STM32F427VI firmware retrieval
Hi All,
Been reading and learning a lot about MCU's in general. I'm very very new to all of this so please bare with me.
The board comes with STM32F427, and a custom .exe that can flash directly via USB-C. I've read about fake STM32's, and. I'm not sure if the MCU is genuine or not, but I'm adding the picture so someone can maybe help.
The board comes with Ethernet, 3 USB-A, 1 USB-C (act as UART maybe?)
The custom .exe can be flashed via USB-C after I put it in DFU mode I presume? (I hold the boot, it flashes blue to allow the flashing). I can click on flash, restore, or even backup basic configs.
I would like to duplicate or retrieve the firmware so I can test it in another board. I tried STM32Cube, ESPtools, and many others, but it doesn't seem to recognize any connectivity.
Any help or guidance would be appreciate.
Thanks.