STM32F446 starting squence
Hi everybody,
I've two cards with a STM32F446 on them.
My first one works very well, the µc starts a each time.
On the second card, the µc starts sometimes (I have a LED on my card that blinks at start).
I've checked Vcap (2.2µF), the 3V3 rising (1ms), boot is well connected to GND with a 10k resistor.
I cannot see what happens in debug mode, because in debug mode , it starts everytime.
Is there a mean to check something else ?
I don't understand what happens.
If you have some ideas...
Thank you.