Stm32f446re CAN start error
CAN Bus Not Starting - HAL_CAN_Start() Error (0x00020000)
Post:
I'm facing an issue where my CAN bus does not start. Tera Term shows the following messages:
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_CAN1_Init();
MX_TIM6_Init();
MX_USART2_UART_Init();
/* USER CODE BEGIN 2 */
filter_config();
HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO0_MSG_PENDING);
sprintf(msg, "CAN1 Instance Address: 0x%08lX\n", (uint32_t)hcan1.Instance);
HAL_UART_Transmit(&huart2, (uint8_t *)msg, strlen(msg), HAL_MAX_DELAY);
if (HAL_CAN_Start(&hcan1) != HAL_OK)
{
sprintf(msg, "CAN Error Code: 0x%08lX\n", HAL_CAN_GetError(&hcan1));
if (HAL_UART_Transmit(&huart2, (uint8_t *)msg, strlen(msg), HAL_MAX_DELAY) != HAL_OK)
{
Error_Handler();
}
Error_Handler();
}
I have already checked the following:
:heavy_check_mark:CAN1 initialization (MX_CAN1_Init())
:heavy_check_mark:Notifications (HAL_CAN_ActivateNotification)
:heavy_check_mark:Debugging in STM32CubeIDE