Skip to main content
Graduate II
July 17, 2024
Solved

Stm32f469i Display is splitted in 4 Rectangles

  • July 17, 2024
  • 1 reply
  • 809 views

Hello,

I'm currently trying to program an STM32F469I-Discovery REV-B-01. I'm using the BSP files from STM32Cube_FW_F4_V1.28.0.

What I want: Just a white screen with "Hello World" at the top.

 

What I'm facing: Look at the picture.

 

This is my Code: 

 BSP_LCD_Init();
 BSP_TS_Init(800,480);

 BSP_LCD_LayerDefaultInit(0, 0xC0000000);
 BSP_LCD_SelectLayer(0);
 BSP_LCD_DisplayOn();
 BSP_LCD_Clear(((uint32_t) 0xFFFFFFFF));
 BSP_LCD_SetBackColor(((uint32_t) 0x00000000));
 BSP_LCD_SetTextColor(((uint32_t) 0xFFFFFFFF));
 sFONT *myfont = &Font24;
 BSP_LCD_SetFont(myfont);

 BSP_LCD_Clear(LCD_COLOR_BLACK);
 BSP_LCD_DisplayStringAt(0, 0, (uint8_t *)"Hello World", 0x01);
 HAL_GPIO_WritePin(LED1_GPIO_Port, LED1_Pin, GPIO_PIN_SET);

 

DerFreaker_0-1721208486726.jpeg

 

    This topic has been closed for replies.
    Best answer by KDJEM.1

    Hello @DerFreaker ,

    May be this example provided in the STM32CubeF4 firmware package help you: STM32Cube_FW_F4_V1.28.0\Projects\STM32469I-Discovery\Applications\STemWin

    Please check the application note AN4323 for detailed steps on using the STemWin library.

    Thank you.

    Kaouthar

    1 reply

    KDJEM.1Answer
    Technical Moderator
    July 19, 2024

    Hello @DerFreaker ,

    May be this example provided in the STM32CubeF4 firmware package help you: STM32Cube_FW_F4_V1.28.0\Projects\STM32469I-Discovery\Applications\STemWin

    Please check the application note AN4323 for detailed steps on using the STemWin library.

    Thank you.

    Kaouthar