Skip to main content
Visitor II
May 25, 2021
Solved

STM32F7, H7: Where can I find info from which APB bus is a given timer clocked?

  • May 25, 2021
  • 5 replies
  • 2607 views

Hello!

For some time already I cannot find this in manuals. Can someone point me if there is any table somewhere? Of course I can find it out experimentally, but it would be more convenient to know where it is listed.

    This topic has been closed for replies.
    Best answer by Peter BENSCH

    The mapping is contained in the table Register boundary addresses, usually in section 2 of the Reference Manual. In addition to the border addresses, it also contains the responsible bus.

    Good luck!

    If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

    /Peter

    5 replies

    Technical Moderator
    May 25, 2021

    The mapping is contained in the table Register boundary addresses, usually in section 2 of the Reference Manual. In addition to the border addresses, it also contains the responsible bus.

    Good luck!

    If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

    /Peter

    WowaAuthor
    Visitor II
    May 25, 2021

    Thank you very much! For sure I wouldn't find this place myself :)).

    Super User
    May 25, 2021

    This is what I've asked several times as a CubeMX feature: for each timer, please show where its clock comes from. Even more, show the current clock frequency from the clock config view.

    Super User
    May 25, 2021

    You could add it as an Idea, to be ignored by ST over there.

    JW

    Graduate
    June 3, 2023

    I opened the RM but looked over it, for those not awake in the morning this visual :):


    _legacyfs_online_stmicro_images_0693W00000dJxUJQA0.png

    Visitor II
    May 18, 2024

    In RM0433 which I am using for the STM32H753, the timer clocking can be determined by the RCC_APB1LRSTR and RCC_APB2RSTR register definitions in Section 8.8, Table 84.