Skip to main content
Visitor II
February 26, 2025
Question

STM32F746G-DISCO screen goes blank when generating PWM signals

  • February 26, 2025
  • 2 replies
  • 434 views

Hello everyone! I have been trying to do a project where I try to control a PWM signal with the touchscreen I made with TouchGFX on my STM32F746G-DISCO, unfortunately, after generating a PWM signal, the screen just goes blank, it doesn't turn off, it just goes completely white. I tried different TIM pins, different configurations and different duty cycles.

Is there something I'm missing? I need to generate at least 2-3 PWM signals and if I am unable to do it with this then I have to use something completely different, I am new to all this so I don't know as much, I can give more information as neccesary!

    This topic has been closed for replies.

    2 replies

    Super User
    February 27, 2025

    PWM should be asynchronous to whatever else the CPU is doing. It's possible it could be causing cross-talk or other interference which is disturbing the video signals. Change PWM frequency to something very slow and see. Ensure you are not calling interrupts at a high rate which will starve the system of cpu resources.

    Graduate II
    February 27, 2025

    From what I can see, on this board the pin LCD_BL_CTRL (PK3) does not map to any of the timer outputs for PWM generation.

    I suppose you could maybe generate the PWM via Hardware Timer on another pin and modify the board to link that to LCD_BL_CTRL (PK3)?