Question
stm32f756 CAN Communication
I am trying to communicate with CAN, but it seems that I am not receiving Rx. I would like to know the reason for this
static void MX_CAN2_Init(void)
{
/* USER CODE BEGIN CAN2_Init 0 */
/* USER CODE END CAN2_Init 0 */
/* USER CODE BEGIN CAN2_Init 1 */
/* USER CODE END CAN2_Init 1 */
hcan2.Instance = CAN2;
hcan2.Init.Prescaler = 5;
hcan2.Init.Mode = CAN_MODE_NORMAL;
hcan2.Init.SyncJumpWidth = CAN_SJW_1TQ;
hcan2.Init.TimeSeg1 = CAN_BS1_8TQ;
hcan2.Init.TimeSeg2 = CAN_BS2_1TQ;
hcan2.Init.TimeTriggeredMode = DISABLE;
hcan2.Init.AutoBusOff = ENABLE;
hcan2.Init.AutoWakeUp = DISABLE;
hcan2.Init.AutoRetransmission = DISABLE;
hcan2.Init.ReceiveFifoLocked = DISABLE;
hcan2.Init.TransmitFifoPriority = DISABLE;
if (HAL_CAN_Init(&hcan2) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN CAN2_Init 2 */
CAN_FilterTypeDef FilterConfig;
FilterConfig.FilterBank = 14;
FilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;
FilterConfig.FilterScale = CAN_FILTERSCALE_32BIT;
FilterConfig.FilterIdHigh = 0x0000;
FilterConfig.FilterIdLow = 0x0000;
FilterConfig.FilterMaskIdHigh = 0x0000;
FilterConfig.FilterMaskIdLow = 0x0000;
FilterConfig.FilterFIFOAssignment = CAN_RX_FIFO0;
FilterConfig.FilterActivation = ENABLE;
FilterConfig.SlaveStartFilterBank = 14;
if (HAL_CAN_ConfigFilter(&hcan2, &FilterConfig) != HAL_OK)
{
/* Filter configuration Error */
Error_Handler();
}
if (HAL_CAN_Start(&hcan2) != HAL_OK)
{
// Start Error
Error_Handler();
}
if (HAL_CAN_ActivateNotification(&hcan2, CAN_IT_RX_FIFO0_MSG_PENDING) != HAL_OK)
{
// Notification Error
Error_Handler();
}
if(HAL_CAN_GetRxFifoFillLevel(&hcan2, CAN_RX_FIFO0) != HAL_OK)
{
/* Reception Missing */
Error_Handler();
}
// HAL_CAN_ConfigFilter(&hcan2, &FilterConfig);
// HAL_CAN_ActivateNotification(&hcan2, CAN_IT_RX_FIFO0_MSG_PENDING);
/* USER CODE END CAN2_Init 2 */
}
initiail Code and i use Can2 port
void HAL_CAN_RxFifo0MsgPendingCallback(CAN_HandleTypeDef *hcan)
{
if ( HAL_CAN_GetRxMessage(hcan, CAN_RX_FIFO0, &Can2RxHeader, canRxBuffer) != HAL_OK)
{
// Error_Handler();
printf( "faild read message.. \r\n");
}
else
{
printf(" Data : %d, %d, %d, %d",canRxBuffer[0],canRxBuffer[1],canRxBuffer[2],canRxBuffer[3]);
}
void Can2Task(void const * argument)
{
// CAN_TxHeaderTypeDef Can2TxHeader;
uint32_t PreviousWakeTime = osKernelSysTick();
uint32_t Tx2MailBox;
uint32_t id, rtr;
CAN_TxHeaderTypeDef Tx2Header;
// CAN_RxHeaderTypeDef Can2RxHeader;
// canTxBuffer[] =
Can2TxHeader.StdId = 0x321;
Can2TxHeader.ExtId = 0x01;
Can2TxHeader.RTR = CAN_RTR_DATA;
Can2TxHeader.IDE = CAN_ID_STD;
Can2TxHeader.DLC = 8;
Can2TxHeader.TransmitGlobalTime = DISABLE;
CanFilter2.FilterBank = 15;
CanFilter2.FilterMode = CAN_FILTERMODE_IDMASK;
CanFilter2.FilterScale = CAN_FILTERSCALE_16BIT;
CanFilter2.FilterIdHigh = 0x106 << 5;
CanFilter2.FilterIdLow = 0x106 << 5;
CanFilter2.FilterMaskIdHigh = 0x7f3 << 5;
CanFilter2.FilterMaskIdLow = 0x7f3 << 5;
CanFilter2.FilterFIFOAssignment = CAN_RX_FIFO0;
CanFilter2.FilterActivation = ENABLE;
CanFilter2.SlaveStartFilterBank = 14;
HAL_CAN_Start(&hcan2);
// if( HAL_CAN_Start(&hcan2) != HAL_OK )
// {
// Error_Handler();
// }
for(;;)
{
osDelayUntil(&PreviousWakeTime, 500UL);
#if 0 // Tx..
if ( HAL_CAN_AddTxMessage(&hcan2 , &Can2TxHeader , canTxBuffer, &Tx2MailBox) != HAL_OK)
{
printf("can send fail..\r\n");
}
else
{
printf(" can send success !! \r\n");
}
#else // Rx..
HAL_CAN_RxFifo0MsgPendingCallback(&hcan2);
#endif
}
}