Skip to main content
Visitor II
May 30, 2024
Question

STM32F765 can use stlink to burn firmware via SWD, but can't access bootloader.

  • May 30, 2024
  • 1 reply
  • 842 views

I am building a circuit board using STM32F765. After building it I can use stlink to burn the firmware (stm32 utility) via SWD and read the chip correctly, but I can't get into the bootloader and I can't use the serial port (USB) to read the chip on my PC.
Make sure the power supply is normal. I'm not sure what's going on here.

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    June 25, 2024

    Dear @yushangchen ,

    Can you give more details with a log when booting from Internal bootloader with BOOT0 pins ? and use the STM32CubeProgrammer either via UART or USB ( DFU).

    Some hints :

    0) Picture of the top marking and revision

    1) Let us know the schematics and especially the  used crystal HSE XXMHz.

    2) try to measure the HSI - Internal 16MHz RC used in the internal booloader and output via a code in flash on MCO - PA8 pin.

    Hope it helps.

    STOne-32.