STM32F767 QSPI Slave
Hi,
I have the following questions about QSPI in STM32F767:
1. Is it possible to configure the board as QSPI Slave? I could not find any option in the CubeMX Tool to choose between master and slave.
2. Is the QSPI peripheral of this board strictly limited to interfacing only QSPI flash devices? In other words, is it possible to interface a QSPI slave which is not a flash device?
3. Is it possible to configure the normal SPI peripheral to work as QSPI?
I referred the below link, which states that QSPI is strictly master-driven. But I would like to confirm this statement.