STM32F767ZI SPI communication with accelerometer LIS2DW12 does'nt work
Hello,
I use STM32F767ZI (on a board NUCLEO-F767ZI) , CubeIDE, HAL driver and I try to communicate with an accelerometer (LIS2DW12 on the board SEN0405) with SPI interface. I'll try to give the more details possible so that you can help me a maximum.
To test the communication between my microcontroller and my accelerometer, I try to read the WHO_AM_I register of the LIS2DW12. This register is a read-only register. Its value is fixed at 44h. Unfortunately I can't read this value but I read FFh. First of all, so that you can confirm that I haven't made an error of connection, here's how I connected my accelerometer to my nucleo-board :
I just connected the accelerometer to the supply (+3.3V & GND) and the 4 SPI wires.
Then, I configured the SPI communication in CUBEMX according to the LIS2DW12 datasheet :


I wrote a simple code to read value of the register WHO_AM_I using the function HAL_SPI_TransmitReceive. According to the datasheet, to read this register (address 0Fh), it must be sent a byte with the value of the address register and a 1 as MSB -> 8Fh.

Here is a part of my code, where I try to read and the SPI configuration below :
uint8_t TxData[2] = {0x8F, 0x00};
uint8_t RxData[2] = {0x00, 0x00};
HAL_SPI_TransmitReceive(&hspi1, TxData, RxData, 2, 200);
/**
* @brief SPI1 Initialization Function
* @PAram None
* @retval None
*/
static void MX_SPI1_Init(void)
{
/* USER CODE BEGIN SPI1_Init 0 */
/* USER CODE END SPI1_Init 0 */
/* USER CODE BEGIN SPI1_Init 1 */
/* USER CODE END SPI1_Init 1 */
/* SPI1 parameter configuration*/
hspi1.Instance = SPI1;
hspi1.Init.Mode = SPI_MODE_MASTER;
hspi1.Init.Direction = SPI_DIRECTION_2LINES;
hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
hspi1.Init.CLKPolarity = SPI_POLARITY_HIGH;
hspi1.Init.CLKPhase = SPI_PHASE_2EDGE;
hspi1.Init.NSS = SPI_NSS_SOFT;
hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_32;
hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi1.Init.CRCPolynomial = 7;
hspi1.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;
hspi1.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;
if (HAL_SPI_Init(&hspi1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN SPI1_Init 2 */
/* USER CODE END SPI1_Init 2 */
}
void HAL_SPI_MspInit(SPI_HandleTypeDef* hspi)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
if(hspi->Instance==SPI1)
{
/* USER CODE BEGIN SPI1_MspInit 0 */
/* USER CODE END SPI1_MspInit 0 */
/* Peripheral clock enable */
__HAL_RCC_SPI1_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
/**SPI1 GPIO Configuration
PA5 ------> SPI1_SCK
PA6 ------> SPI1_MISO
PA7 ------> SPI1_MOSI
*/
GPIO_InitStruct.Pin = GPIO_PIN_5|GPIO_PIN_6|GPIO_PIN_7;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_MEDIUM;
GPIO_InitStruct.Alternate = GPIO_AF5_SPI1;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/* USER CODE BEGIN SPI1_MspInit 1 */
/* USER CODE END SPI1_MspInit 1 */
}
}
After executing my code, my RxData contains two FFh bytes. I don't know where I did something wrong, if someone have any idea, help me please thank you !