Skip to main content
Explorer
May 6, 2025
Solved

STM32F769 VDDUSB

  • May 6, 2025
  • 2 replies
  • 338 views

Hello,
I'm using in my projects with ports PA10,PA11 (for Logs - uart), and PB14 and PB15 as normal GPIO.
They didn't works.

After long troubleshooting.... I found out that is because these ports are supply separately by the VDDUSB pin which was disconnected.

I couldn't find the reason in the datasheet, I'll be happy to understand the construction and the reason. 

 

    This topic has been closed for replies.
    Best answer by AScha.3

    Hi,

    reason...ask chip designer, why separate VddUSB ...maybe, to be more flexible, if chip runs on 1,8V, the USB related pins still have to work on 3v3 ; so can supply separate, if needed;

    and see ds :  General operating conditions

    AScha3_0-1746521704785.png

     

    2 replies

    AScha.3Answer
    Super User
    May 6, 2025

    Hi,

    reason...ask chip designer, why separate VddUSB ...maybe, to be more flexible, if chip runs on 1,8V, the USB related pins still have to work on 3v3 ; so can supply separate, if needed;

    and see ds :  General operating conditions

    AScha3_0-1746521704785.png

     

    UB40Author
    Explorer
    May 6, 2025

    thank you