Skip to main content
Visitor II
April 19, 2024
Solved

STM32G0 Reference Manual Typo (ADC-Oversampler)

  • April 19, 2024
  • 1 reply
  • 945 views

RM0444 (Rev. 5 Nov 2020 - should be newest):

Chapter 15.8 Oversampler: "N is defined using the OVFS[2:0] bits": this should say "OVSR[2:0]" bits.

Chapter 15.12.3: Register ADC_CR Note for AD_EN: "set ADEN only when all bits of ADC_CR registers are 0" should better say: "set ADEN only when all bits of ADC_CR register except ADVREGEN are 0"

Chapter 15.12.5: Register ADC_CFGR2 A warning hint/Note for OVSR[2:0] would be nice, e. g. : Note: ADC_DR truncates to 16bit (set OVSS to 1-4 shifts for OVSR values 4..7 (32x...256x)).

    This topic has been closed for replies.
    Best answer by STTwo-32

    Hello @flyer31 

    Thank you for your contribution. I've escalate this internally for correction for the first proposition and for reviewing by the doc owner for the other two points (under internal ticket number 179616).

    Best regards.

    STTwo-32

    1 reply

    STTwo-32Answer
    Technical Moderator
    April 19, 2024

    Hello @flyer31 

    Thank you for your contribution. I've escalate this internally for correction for the first proposition and for reviewing by the doc owner for the other two points (under internal ticket number 179616).

    Best regards.

    STTwo-32