STM32G071: TIM1+PWM+DMA 2nd pulse looks strange
Hi,
I'm trying to talk to WS2812 RGB Leds. I'm using TIM1 CH3 PWM Output with DMA. Everything looks almost fine. I'm always sending the same data using:
HAL_TIM_PWM_Start_DMA (&htim1, TIM_CHANNEL_3, (uint32_t *) pwmData, (24 * NUM_OF_LEDS) + 50);Here pwmData sets a duty cycle of 33 % (20 of period 60, 48 MHz) for the first 13 cycles. In between I wait for 500 ms.
But time to time (~1 out of 3) the second pulse behaves strange. Only the second pulse seems to randomly jump approx. from duty cycle 20 ... 80 %. All remaining pulses are correct.
Thanks for any hint!