STM32G071GBUx Bootloader Setup Problem
Hi, I am trying to configure my STM32G071GBU6 to enable reprogramming the flash throguh USART1. I check the datasheet of STM32G071x8/xB, reference manual RM0444, and application note AN2026. It says I am supposed to configure the PA9 (USART1_Tx) and PA10 (USART1_Rx) pins. The problem is when I configure the USART1 as asynchronous mode in STM32CubeMX, the software automatically set PB6 and PB7 pins as USART1_Tx and USART1_Rx. There are no available options like USART1_Tx and USART1_Rx for PA9 and PA10.
I am wondering why the manual is inconsistent to the STM32CubeMX and how should I configure the MCU to correctly reprogram through USART1?