Skip to main content
Graduate
May 6, 2024
Solved

STM32G0C1RET6(ARM® Cortex®-M0+ STM32G0 Microcontroller IC 32-Bit Single-Core 64MHz 512KB (512K x 8))

  • May 6, 2024
  • 1 reply
  • 745 views

Hi,

          (STM32G0C1RET6  for this part number ARM® Cortex®-M0+ STM32G0 Microcontroller IC 32-Bit Single-Core 64MHz 512KB (512K x 8) FLASH 64-LQFP (10x10))

two type of pin descriptions have mentioned in the datasheet, I confused which one I have to take for "STM32G0C1RET6" this part and which pin I will for watchdog timer so kindly help me. Find the screenshot for your reference.

 

lqfp.png

 

    This topic has been closed for replies.
    Best answer by Peter BENSCH

    This is explained in section 4 of the data sheet:

    The devices housed in 32-pin, 48-pin, and 64-pin packages come in two variants - “GP” and “N” (the latter with ordering code having N behind the temperature range digit).

    Hope that answers your question?

    Regards
    /Peter

    1 reply

    Technical Moderator
    May 6, 2024

    This is explained in section 4 of the data sheet:

    The devices housed in 32-pin, 48-pin, and 64-pin packages come in two variants - “GP” and “N” (the latter with ordering code having N behind the temperature range digit).

    Hope that answers your question?

    Regards
    /Peter