STM32G4 CAN TX buffer
Hello,
I'am currently programming on a STM32G473. I'am sending CAN Message via the FDCAN peripheral.
In generally everything works, all my messages I put into the Tx Buffer are sent.
But in one little detail I'am confused:
In Figure 669 its described, that the TX buffer consists of 3 elements.
But if I want to find out in which index I have to put the next message by reading the TXFQS_TFQPI field, I'am confused why the reference manual describes a range of 0-3 for this field. So it seems that there are 4 messages? But in the Add-Request Register (TXBAR_AR) there are only 3 Bits for adding transmission requests (and the RAM buffer has only space for 3 Messages).
- If the put index is 0 --> I set the Bit 0 in TXBAR_AR
- If the put index is 1 --> I set the Bit 1 in TXBAR_AR
- If the put index is 2 --> I set the Bit 2 in TXBAR_AR
- If the put index is 3 --> What should I do? There is no bit for a fourth request (and also no space in Buffer for a fourth message)
So is it maybe an error in the reference manual and the range of TXFQS_TFQPI is only 0-2 and in reality the peripheral will never give me a 3 in this field?
Or, if the range 0-3 is correct: What should I do if I get a put-Index of 3?
[Ref: RM0440, Rev. 8]