STM32G4 DAC DMA double data
I can produce a sine wave using DAC1 + DMA on a STMG431CBU6 MCU, but I'd like to increase the frequency (purely as a learning exercise). In the application note https://www.st.com/resource/en/application_note/an4566-extending-the-dac-performance-of-stm32-microcontrollers-stmicroelectronics.pdf it suggests that the DAC update rate can be increased by using DMA Double Data mode. When I enable double data mode in STM32CubeIde, however, the generated sine wave frequency is halved and an additional high frequency signal is superimposed on it.
DAC settings (DMA double data enabled):

Sine wave generated when DMA double data is disabled:

Sine wave generated when DMA double data is enabled:

'Close-up' of the superimposed signal:

From this image the superimposed signal frequency seems to be ~6.17 MHz.
I presume there is more to enabling DMA double data mode than changing the DAC setting in STM32CubeIDE, but I haven't been able to find anything else. Can anyone tell me where I have gone wrong or what else I need to do?